990-71222-001

Storage Conditions

Storage temperature:
-25 °C to 55 °C (-13 °F to 131 °F) 

Relative humidity:
10-80% non-condensing

Altitude:
0-10000 m (0-32000 ft)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?