990-71222-001

UPS Shipping Weights and Dimensions

Commercial reference Weight kg (lbs) Height mm (in) Width mm (in) Depth mm (in) Number of preinstalled power modules in the UPS Number of power modules shipped separately* Number of extra power modules that can be ordered*
GVL0K500DS 468 (1032) 2145 (84.4) 950 (37.4) 1100 (43.3) 0 0 10
GVL200K500DS 620 (1367) 2145 (84.4) 950 (37.4) 1100 (43.3) 4 0 6
GVL300K500DS 620 (1367) 2145 (84.4) 950 (37.4) 1100 (43.3) 4 2 4
GVL400K500DS 620 (1367) 2145 (84.4) 950 (37.4) 1100 (43.3) 4 4 2
GVL500KDS 620 (1367) 2145 (84.4) 950 (37.4) 1100 (43.3) 4 6 0

Power Module Shipping Weights and Dimensions

Commercial reference Weight kg (lbs) Height mm (in) Width mm (in) Depth mm (in)
GVPM50KD 62 (137) 330 (13) 580 (22.8) 780 (30.7)
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?