990-6512A-001

Connect the Power and Signal Cables

  1. Connect the non-SELV/non-Class 2 signal cables to the terminal block (1-10) and torque to 0.5-0.6 Nm (0.36-0.44 lb-ft / 4.42-5.31 lb-in). Route the signal cables out through the bottom of the remote alarm panel and connect in the UPS. Use 20 AWG multicore signal cables. Note that terminals 9-10 are only relevant for connection to GVSUPS20K100B3H – see UPS installation manual for details.
  2. Connect the provided signal cables 0W49487 and 0W49491 to the terminal block (11-14) and torque to 0.5-0.6 Nm (0.36-0.44 lb-ft / 4.42-5.31 lb-in). Route the signal cables out through the bottom of the remote alarm panel, and connect to the load equipment. The provided signal cables are 30 m (98.4 ft) long.
  3. Remove the warning label from the power terminals.
  4. Connect the power supply cables to the power terminals (phase, N and ground). Power source must be 110-240 VAC. Use 20 AWG 3-core cables.
  5. Reinstall the warning label over the power terminals.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.