990-6512A-001

Mount the Remote Alarm Panel to the Wall

CAUTION
Risk of injury or equipment damage
  • Mount the remote alarm panel to a wall or a rack that is structurally sound and able to support the weight of the unit.
  • Use appropriate hardware (not supplied) to mount the remote alarm panel to the wall.
Failure to follow these instructions can result in injury or equipment damage.
NOTE: Four M8 x 30 torx and nuts are supplied for mounting the remote alarm panel to a rack.
  1. Measure and mark the four mounting hole locations on the wall.
  2. Drill holes in each of the four marked locations.
  3. Mount the remote alarm panel to the wall.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.