990-72555-001

UPS with Internal Batteries Up to 2 Battery Strings

UPS Shipping Weights and Dimensions

  Weight kg (lbs) Height mm (in) Width mm (in) Depth mm (in)

UPS with one battery string

270 (595)

1680 (66.14)

640 (25.19)

990 (38.98)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.