Connect the Power Cables
![]() |
---|
hazard of electric shock, explosion, or arc flash
Perform a total power off of the UPS system before connecting
the battery cables to the battery breaker box.
Failure to follow these instructions will result in death or serious injury.
|
![]() |
---|
Hazard of electric shock, explosion, or arc flash
For TT and TN systems each stand alone cabinet of the
system must be individually connected to the protective earthing terminal
in the distribution board that supplies the system.
Failure to follow these instructions will result in death or serious injury.
|
![]() |
---|
Hazard of arc flash
Use the provided M10 bolts and nuts to connect the power
cables.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
- Lockout/Tagout the battery breaker.
- Route the PE cables from the UPS into the battery breaker box as shown and connect.
- Route the DC cables from the UPS into the battery breaker
box as shown and connect.
DANGER
Hazard of electric shock, explosion, or arc flashReinstall the top protection cover on the battery breaker(s) before continuing with the installation.Failure to follow these instructions will result in death or serious injury. - Route the battery cables from the battery bank through
the bottom of the battery breaker box and connect.
DANGER
hazard of electric shock, explosion, or arc flash- Reinstall the bottom protection cover on the battery breaker(s) before continuing with the installation.
- Ensure correct polarity.
Failure to follow these instructions will result in death or serious injury. - Attach the cables to the cables reliefs in the left side, the top, and the bottom of the battery breaker box.