990-6161A-001

Connect the Power Cables for a UPS Rated for Maximum 100 kW

NOTICE
Risk of equipment damage
Only connect the DC cables from battery breaker to battery breaker in installations with a UPS rated for maximum 100 kW. For installations with a UPS rated over 100 kW, see Connect the Power Cables for a UPS Rated over 100 kW.
Failure to follow these instructions can result in equipment damage.
  1. Connect the preinstalled PE cables (0W50448) between the modular battery cabinets as shown.
  2. Connect the preinstalled DC cables (0W50425) between the modular battery cabinets as shown. Connect DC- to DC- and connect DC+ to DC+ between the modular battery cabinets.
    NOTE: The preinstalled DC cables come in pairs: Two cables for DC- connection and two cables for DC+ connection. Ensure to connect all pairs between the modular battery cabinets.

    Front Left View of the Modular Battery Cabinet

    Front Right View of the Modular Battery Cabinet

    Top View of the Modular Battery Cabinets

  3. For installation with adjacent UPS: Follow the UPS installation manual to connect the PE and DC cables in the UPS.
  4. For installation with remote UPS:
    1. Optional: You can remove the right side panel from modular battery cabinet 1 for easier access. Reinstall the side panel after power cabling is completed.
    2. Disconnect the preinstalled PE cable and DC cables from modular battery cabinet 1. The preinstalled power cables are not long enough for connection to a remote UPS.
    3. Connect the PE cable and the DC cables (not provided) in modular battery cabinet 1.
    4. Route the PE and DC cables out through the conduit box and into the UPS power cabling area.
    5. Follow the UPS installation manual to connect the PE and DC cables in the UPS.

    Front Left View of Modular Battery Cabinet 1

    Front Right View of Modular Battery Cabinet 1

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.