990-6161A-001

Installation Procedure for UPS for External Batteries

NOTE: The modular battery cabinet can only be installed remote to a UPS for external batteries.

Modular Battery Cabinets and Remote UPS Rated for Maximum 100 kW

Two Modular Battery Cabinets and Remote UPS Rated over 100 kW

Three Modular Battery Cabinets and Remote UPS Rated over 100 kW

Four Modular Battery Cabinets and Remote UPS Rated over 100 kW

NOTE: The distance between the modular battery cabinet(s) and the UPS must not exceed 100 m. Contact Schneider Electric for installations with a longer distance.
  1. Prepare for Installation.
  2. Install the Conduit Box on the Modular Battery Cabinet.
  3. Prepare Modular Battery Cabinet 1 for Signal Cables.
  4. Install the Seismic Anchoring (Option).
  5. Interconnect the Modular Battery Cabinets.
  6. Perform one of the following:
  7. Connect the Signal Cables.
  8. Add Translated Safety Labels to Your Product.
  9. Final Installation.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.