990-72555-001

Storage Conditions

Storage temperature:
For UPS for external batteries:
-25 °C to 55 °C (-13 °F to 131 °F) 
For UPS with internal batteries:
-15 °C to 40 °C (5 °F to 104 °F) 

Relative humidity:
0-95% non-condensing

Altitude:
0-10000 m (0-32000 ft)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?