990-5783K-034

Galaxy VX1500 kW G/Ç Kabini ile UPSKurulum

380 V, 400 V, 415 V, 440 V, and 480 V

1100 kW/kVA and 1100 kW/kVA N+1
500 kW/kVA, 750 kW/kVA, and 1000 kW/kVA Expandable to 1250 kW/kVA, 1250 kW/kVA, 1250 kW/kVA, 1250 kW/kVA N+1
500 kW/kVA, 750 kW/kVA, 1000 kW/kVA, and 1250 kW/kVA Expandable to 1500 kW/kVA, 1500 kW/kVA, 1500 kW/kVA N+1

4/2025

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Bu yardımcı oldu mu?