990-91375D-001

Installation Procedure

DANGER
hazard of electric shock, explosion or arc flash
Place the battery breaker box as close to the battery bank as possible to limit the length of unprotected battery cable. The distance between the battery bank and the UPS must not exceed 200 m. Contact Schneider Electric for installations with a longer distance.
Failure to follow these instructions will result in death or serious injury.
NOTE: Installation of the battery temperature sensor is not described in this manual, see the UPS installation manual for details.
  1. Mount the Battery Breaker Box to the Wall.
  2. Prepare the Battery Breaker Box for Cables.
  3. Connect the signal cables. Perform one of the following procedures:
  4. Connect the Power Cables.
  5. Add Translated Safety Labels to Your Product.
  6. Final Installation Steps.
For moving or decommissioning the battery breaker box after installation has been completed, see Decommission or Move the Battery Breaker Box to a New Location.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.