990-91375D-001

Prepare the Battery Breaker Box for Cables

DANGER
Hazard of electric shock, explosion, or arc flash
Do not drill or punch holes for cables or grommets with the gland plates installed, and do not drill or punch holes in close proximity to the UPS.
Failure to follow these instructions will result in death or serious injury.
  1. Remove the gland plates:
    • For GVBBB630EL-1CB: Remove the bottom gland plates.
    • For GVBBB630EL-2CB: Remove the top and bottom gland plates or only the bottom gland plates.
    • For GVBBB630EL-3CB: Remove the top and bottom gland plates.

    GVBBB630EL-1CB

     

    GVBBB630EL-2CB and GVBBB630EL-3CB

    GVBBB630EL-2CB and GVBBB630EL-3CB

  2. Drill or punch holes for power cables (A) and signal cables (B) or grommets in the gland plates, install grommets (if applicable), and reinstall the gland plates.
    DANGER
    hazard of electric shock, explosion, or arc flash
    Ensure that there are no sharp edges that can damage the cables.
    Failure to follow these instructions will result in death or serious injury.

    GVBBB630EL-1CB

     

    GVBBB630EL-2CB and GVBBB630EL-3CB

    GVBBB630EL-2CB and GVBBB630EL-3CB

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.