EIO0000004948.02

Allowlisting

Zero-day cybersecurity attacks take place before a software vendor is aware of a cybersecurity exploit. Meaning that neither software, nor anti-virus programs have been created or updated to protect against the zero-day threat or attack.

Application allowlisting is recommended to protect against zero-day attacks. This specifies an index of approved software applications and processes that are permitted to be present and active on the operating system.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?