EIO0000004948.02

Security Practices for Removable Devices

When using removable devices such as external hard drives or USB drives, refer to the following recommended actions to protect against unauthorized access and unintended disclosure of data.
  • Scan any devices used to exchange data before using them in any node connected to the network.

  • Encrypt your files.

  • Use password protection.

  • Do not store sensitive data in removable media, or if you need to store sensitive data in removable media, manage it properly in a secure location.

  • Disable unused ports or limit available devices.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?