Firmware Update with EcoStruxure Power Commission Software
Use the latest version of EcoStruxure Power Commission software to update I/O Smart Link to the latest firmware version available.
The latest version of EcoStruxure Power Commission software is available at www.se.com.
For more information about the use of EcoStruxure Power Commission software, refer to EcoStruxure Power Commission Online Help.
The following table indicates the reference duration of the I/O Smart Link firmware upgrade.
Baud rate | Duration of firmware upgrade using EcoStruxure Power Commission via: | |
---|---|---|
Serial communication | TCP gateway (for example, Panel Server) | |
4800 |
From 12 to 13 minutes |
From 11 to 12 minutes |
9600 |
From 8 to 9 minutes |
From 6 to 7 minutes |
19200 |
From 6 to 7 minutes |
From 4 to 5 minutes |
38400 |
From 5 to 6 minutes |
From 3 to 4 minutes |
57600 |
From 5 to 6 minutes |
From 3 to 4 minutes |
115200 |
From 4 to 5 minutes |
From 2 to 3 minutes |
Note: The values of the above table are only for the reference, actual duration of the firmware upgrade may vary depending on the network operation, network settings, gateway configuration and other infrastructure latencies.