Pulse output

Command Number

Action
(R/W)

Size

Type

Unit

Range

Description

2003

W

1

UInt16

(Reserved)

W

2

Float32

kW/pulse

10000, 2000, 1000, 100, 10, 1, 0.1, 0.01

Pulse constant

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.