Communication

Command Number

Action
(R/W)

Size

Type

Unit

Range

Description

5000

W

1

UInt16

(Reserved)

W

1

UInt16

(Reserved)

W

1

UInt16

(Reserved)

W

1

UInt16

1 – 247

Meter ID (Modbus)

W

1

UInt16

1 – 4

Baud Rate:

  • 1 = 9600
  • 2 = 4800
  • 3 = 2400
  • 4 = 1200

W

1

UInt16

1 – 3

Parity:

  • 1 = Even
  • 2 = None
  • 3 = Odd

W

1

UInt16

(Reserved)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.