Meter Features

The key features of iEM2050 series meter are listed below:
  • Measurement of active and reactive energy,

  • 2 tariffs configured through Modbus communication,

  • Pulse outputs,

  • LCD display (current, voltage, power and energy measurements, and basic configuration),

  • Communication via Modbus.

For applications, feature details and complete specifications of the iEM2050 series meters, see the iEM2050 series technical datasheet at www.se.comwww.usa.siemens.com/pds.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?