Feature summary

Parameter iEM2050 iEM2055
4 quadrant energy measurements
Power:
  • Active power (kW)

  • Apparent power (kVA)

  • Reactive power (kVAR)

Current
Voltage
Frequency
Power factor
2 tariffs configured through Modbus communication
Pulse outputs
Communication RS-485 Modbus RTU RS-485 Modbus RTU
MID compliant
Class 1 as per IEC 62052-11 and IEC 62053-21
Class B as per EN 50470-1/3
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?