PHA8599500-06

Conformité aux normes chinoises

Ce produit est conforme aux normes chinoises suivantes :

BS/EN/IEC 62052-11:2020 Electricity metering equipment (A.C.) - General requirements, tests And test Conditions - Part 11: Metering equipment

BS/EN/IEC 62053-21 Electricity metering equipment (A.C.) - Particular requirements - Part 21: Static meters for active energy (classes 1 and 2)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Contenu utile ?