7EN02-0416-03

Configuring input output parameters

Applicable for IFL12MC, IFL12LMC, IFL12MCT, and IFL12LMCT.
  1. Navigate to Menu > Settings > I/O Config.

    The I/O CONFIG screen displays.

  2. Modify the parameters value as per the following table:
    NOTE: Use the contextual menu buttons to modify the parameters value.
    Parameter Allowed Values Default Value Description
    Ins. Al. Relay
    • Std. (Standard)

    • FS (Failsafe)

    FS (Failsafe) Select the mode of insulation alarm relay depending on the status of insulation. Refer user manual for more information.
    Ack Al. Relay
    • ON

    • OFF

    ON
    • Select ON to trigger relays when acknowledging alarm.

    • Select OFF to disable this feature.

    Test w. Relays
    • ON

    • OFF

    ON
    • Select ON to include a three-second toggle of the preventive insulation alarm relay and insulation alarm relay during a manually launched auto-test.

    • Select OFF to disable this feature.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.