7EN02-0416-03

Configuring insulation alarm parameters (IFL12C)

  1. Navigate to Menu > Settings > Ins. Alarm.

    The INS. ALARM screen displays.

  2. Modify the parameters value as per the following table:
    NOTE: Use the contextual menu buttons to modify the parameters value.
    Parameter Allowed Values Default Value Description
    Ins. Alarm
    • Low

    • Medium

    • High

    Low

    Select the option as per the following:

    • Low: The device detects low-impedance insulation faults.

    • Medium: The device detects medium-impedance insulation faults.

    • High: The device detects high-impedance insulation faults.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.