Replacing the Installation Gasket
| NOTICE |
|---|
|
Failure to follow these instructions can result in equipment damage.
|
| NOTICE |
|---|
|
Failure to follow these instructions can result in equipment damage.
|
Installing the Installation Gasket
- Place this product on a flat, level surface, with the display face pointing down.
- Remove the gasket from this product.
-
Attach the new gasket to this product. Insert the protrusions
from the four corners of the gasket into the corresponding holes in
the corners of this product.
Depending on your model, there may be additional protrusions. In the following, refer to the figure on the right and insert the protrusions accordingly.NOTE: When using a tool to insert the gasket, make sure the tool does not catch the rubber gasket and cause a tear.