Settings Workflow

Follow the steps below to configure the software.
  1. Configure the display settings from the screen properties (Screen Resolution) for your host.
  2. Download and install the utilities onto the host.
    NOTE: To use these utilities, Microsoft® .NET Framework is required. If .NET Framework is not installed, the .NET Framework installation screen will appear. Install following the on-screen instructions.
  3. Start the Launcher.
  4. Configure the utilities as needed, in any order.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?