Safety Precautions
![]() |
---|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, or Arc Flash
Failure to follow these instructions will result in death or serious injury.
|
WARNING: This product can expose you to chemicals including Nickel compounds, which are known to the State of California to cause cancer, and Bisphenol A (BPA), which is known to the State of California to cause birth defects or other reproductive harm. For more information go to www.P65Warnings.ca.gov. |
Moisture Contamination Avoidance and Mitigation
![]() |
---|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
![]() |
---|
Fire Hazard
Remove all flammable material in the vicinity of the heaters,
such as packaging, accessories in boxes, and documentation, before
energizing the heaters.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
Shipping, Receiving, and Storage Requirements
This equipment does not achieve its ratings until it is installed per record/as-built drawings, per the instructions contained in this document, and has operational environmental controls with appropriate settings to help mitigate environmental influences. This equipment can also be stored in a climate-controlled area that uses both heating and cooling to maintain acceptable environmental conditions. Indoor and outdoor rated equipment is not suitable for outdoor storage.
-
Treat the equipment as if it is in storage until it is installed and operational. The storage area must be clean, dry (75% or less relative humidity), and climate-controlled with proper ventilation.
-
To keep the equipment dry, use of heaters is required in some cases (for example, during seasonal or low periods of electrical loading and equipment de-energization).
-
Consult the engineer of record for the appropriate environmental control settings or means to mitigate environmental influences.
-
If so equipped, set the thermostats and/or humidistats to mitigate condensation. A minimum of 200 W of heat per section is recommended.
- If heaters are used with the equipment that were not included in the equipment by Schneider Electric, they must be clean and free of debris and grease. Greasy and/or smoky heaters can contaminate electrical insulation and lead to dielectric breakdown and/or tracking.
-
-
Shipping packaging is not suitable for and cannot be used by itself for equipment storage unless otherwise indicated on the shipping packaging labeling.
-
When receiving equipment, the equipment may be at a lower temperature than the ambient air temperature. Allow time for the equipment temperature, including the temperature of internal components, to rise to the ambient air temperature before making openings in or otherwise disturbing the packaging. Condensation can occur on and inside the equipment if warm air contacts cold surfaces of the equipment. Moisture damage can occur, destroying the dielectric capabilities of the equipment and rendering it unusable.
-
The factory shipping wrap around the equipment on shipping pallets is not suitable for non-enclosed (no tarp) over-the-road transportation that risks exposing the equipment to the elements. Leave the factory shipping wrap around the equipment on the equipment until the equipment is ready for inspection and stored or inspected and installed. After receiving the equipment and allowing it to acclimate to the environment, remove the packaging and inspect the equipment for damage that may have occurred in transit. If damage is found or suspected, immediately file a claim with the carrier and notify your Schneider Electric representative.
-
Follow these guidelines every time the equipment is moved to a new storage location or to its final destination.
Installation, Operation, and Maintenance Requirements
This equipment does not achieve its ratings until it is installed per record/as-built drawings, installed per the instructions contained in this document, and has operational environmental controls with appropriate settings to help mitigate environmental influences. This equipment can also be operated in a climate-controlled area that uses both heating and cooling to maintain acceptable environmental conditions. Indoor and outdoor rated equipment is not suitable for outdoor storage.
In some cases (such as seasonal electrical loading, de-energized equipment, and standby/alternate power sources), the heat generated by equipment loading is insufficient to help prevent condensation and alternate heat sources are required. If environmental controls such as a thermostat or humidistat are used, their settings must be sufficient to mitigate condensation and always remain operational. Consult the engineer of record for the appropriate environmental control settings.
Exposure to Moisture, Chemicals, and Condensation
If liquids such as moisture, chemicals, and condensation contact the electronics, circuit breaker, fuses, bussing, or other electrical components, do not attempt to clean or repair the equipment as this may lead to unrepairable damage. If the equipment is energized, de-energize it. If equipment is not energized, do not energize it. Contact the Schneider Electric Customer Care Center at 888-778-2733.