Circuit Breaker Overview

Presentation

The circuit breaker overview function displays a description of the circuit breaker block, including:

  • Circuit breaker range

  • Device size

  • Rated current

  • Performance level

  • Power system

  • Standard

Data Availability

The circuit breaker overview data is available as follows:

  • On the MicroLogic X display screen at Home > Maintenance > CB overview

  • WithEcoStruxure Power Commission software

  • On a remote controller using the communication network

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?