MicroLogic X Control Unit: Purchasing and Installing a Digital Module

Prerequisites

To purchase a Digital Module, you will need to provide the following information:

  • The MicroLogic X control unit identification number

  • The commercial reference of the Digital Module to be purchased.

  • The email address to receive the Installer email containing Digital Module download information.

Getting Control Unit Identification Number

You can get the control unit identification number on site or off site using one of the following means:

  • On site, by scanning the QR code on the front face of the MicroLogic X control unit from a smartphone. The QR code identifies the MicroLogic X control unit. Use the Share button to share the control unit information with the person qualified to select and purchase Digital Modules.

  • On site, by reading the identification number on the front face of the MicroLogic X control unit. The identification number starts with four zeros and is 16 characters long.

  • On site, from EcoStruxure Power Commission software with a PC connected to the mini USB port of the MicroLogic X control unit.

  • Off site, from EcoStruxure Power Commission software. This access can only be used for a MicroLogic X control unit previously registered in the relevant project.

Purchasing and Downloading a Digital Module

Follow this procedure to purchase and download a Digital Module:

Step Action

1

Contact your local Schneider Electric Customer Care Center (CCC) or Schneider Electric Services representative.

Visit www.se.com/support to contact your local Schneider Electric CCC.

2

Provide the information indicated in Prerequisites and purchase the Digital Module.

You will receive an Installer email at the address you indicated to CCC.

3

Select the email from dsc-no-reply@verified.se.com to download your Digital Module. The subject is Your Digital Modules are ready for download. Your Digital Module appears in a list of items ready to be downloaded.

NOTE: If you do not see the email in your Inbox, check the Junk mailbox.

4

Click the checkbox next to the Digital Module that you want to download and click Download to download the delivery package.

NOTE: This delivery package is used to install the Digital Module on the MicroLogic X control unit using EcoStruxure Power Commission software. Make sure that the delivery package is present on the PC used to install a Digital Module.
NOTE: If the Digital Module was purchased previously, you can access the file downloaded by clicking the following link:

https://digitalpackage.schneider-electric.com/dpb?lang=en.

Installing a Digital Module on the MicroLogic X Control Unit

The MicroLogic X Administrator, Services, or Engineer password is required to install a Digital Module on the MicroLogic X control unit.

Follow this procedure to install a purchased Digital Module on a MicroLogic X control unit.

Step Action
1 Use the USB cable with part number LV850067SP to connect a PC running EcoStruxure Power Commission software to the mini USB port on the front face of the MicroLogic X control unit.
2

Click Connect to device directly to establish a connection between the EcoStruxure Power Commission software and the MicroLogic X control unit. EcoStruxure Power Commission software displays the MicroLogic X control unit identification number on the screen.

3

Open the Digital Module page by clicking Digital Modules.

4

Check that the delivery package for the Digital Module to be installed is present on the PC being used.

5

Select the Digital Module to be installed by clicking Install.

The standard protection functions of the MicroLogic X control unit remain active during installation of the Digital Module.

NOTE: Only modules previously purchased can be installed directly by clicking Install.

6

EcoStruxure Power Commission software asks you to confirm the installation. Enter the Administrator password and click CONTINUE.

7

A message is displayed to indicate that the Digital Module is being installed. Click the cross to continue.

8

When installation is complete and before unplugging the PC, disconnect EcoStruxure Power Commission software from the MicroLogic X control unit by clicking the Disconnect button.

9

Use the EcoStruxure Power Device app to check that the Digital Module is installed.

10

Use the EcoStruxure Power Device app or EcoStruxure Power Commission software to check that the Digital Module is working correctly.

For more information, refer to EcoStruxure Power Commission Online Help.

NOTE: To uninstall a Digital Module, use EcoStruxure Power Commission software.

Predefined Events

The following events are generated when a Digital Module is installed or uninstalled:

Code

Event

History

Severity

0x1130 (4400)

Digital module License installed

Configuration

Low

0x1131 (4401)

Digital module License uninstalled

Configuration

Low

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?