Monitoring the MCH Gear Motor

Presentation

The MCH gear motor undergoes wear due to the number of charging operations. It is recommended to check it at periodic intervals to decide whether the gear motor must be changed or not. To avoid regular inspection of the gear motor, events are generated when the gear motor reaches 80% or 100% of the recommended maximum number of charging operations.

Operating Principle

The MicroLogic X control unit:

  • Counts the number of charging sequences performed to rearm the closing mechanism after each circuit breaker closure.

  • Measures and records the last charging time of the MCH gear motor to rearm the closing mechanism.

  • Calculates the percentage of wear of the MCH gear motor

  • Generates an event when:

    • MCH gear motor reaches 80% of recommended maximum number of charging operations

    • MCH gear motor reaches 100% of recommended maximum number of charging operations

For more information about the recommended number of operations, refer to DOCA0099•• MasterPacT MTZ - IEC Switch-Disconnectors and Circuit Breakers with MicroLogic X Control Unit - Maintenance Guide.

Resetting the MCH Gear Motor Data

NOTICE
invalid monitoring
After replacement of the MCH gear motor, reset the charging operation counter to zero.
Failure to follow these instructions will result in incorrect operation count.

The following MCH gear motor data can be reset or set to zero with EcoStruxure Power Commission software (password-protected):

  • Charging operation counter

  • Last charging time

Data Availability

The MCH gear motor data is available as follows:

  • On the MicroLogic X display screen, at: Home > Maintenance > Health > Actuator wear

  • With EcoStruxure Power Commission software

  • With the EcoStruxure Power Device app through Bluetooth or USB OTG connection

  • On a remote controller using the communication network

Monitoring data MicroLogic X HMI EPC software EPD software Communication

Percentage wear

Yes

No

Yes

No

Charging operation counter

No

Yes

Yes

Yes

Last charging time

No

Yes

Yes

Yes

Predefined Events

The monitoring of the MCH gear motor generates the following events:

Code

Event

History

Severity

0x1450 (5200)

MCH charging operations above threshold

Diagnostic

Medium

0x1451 (5201)

MCH has reached the max number of operations

Diagnostic

High

Recommended Actions

Code

Event

Recommended actions

0x1450 (5200)

MCH charging operations above threshold

Plan to replace the MCH.

0x1451 (5201)

MCH has reached the max number of operations

Replace the MCH.

Contact Schneider Electric Support or your Schneider Electric Services representative for more information about who can carry out the recommended actions.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?