Assistance

Presentation

The assistance menu on the MicroLogic X display screen gives information on the following:

  • Maintenance Schedule

  • Firmware version: The display screen gives information about the firmware version of the microprocessors installed in the MicroLogic X control unit. Firmware updates are managed with EcoStruxure Power Commission software.

  • Hardware version: The display screen gives information about the hardware version of the MicroLogic X embedded display screen in the format aaa.bbb.ccc.

    • If aaa = 001: display screen without IEEE 802.15.4 wireless communication

    • If aaa >= 002: display screen with IEEE 802.15.4 wireless communication

Data Availability

The firmware version is available as follows:

  • On the MicroLogic X display screen, at: Home > Maintenance > Assistance > Firmware version

  • With EcoStruxure Power Commission software

  • With EcoStruxure Power Device app

  • On a remote controller using the communication network

The hardware version is available on the MicroLogic X display screen, at: Home > Maintenance > Assistance > Hardware version

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?