Causes of Aging

@TW: shared topic used in Maintenance Guides: DOCA0305 (MTZ with Mic Act), DOCA0099 (MTZ with Mic X), LVPED508016 (NT/NW)

Introduction

Switchboards and switchgear age whether they are in operation or not. Aging is due primarily to the influence of the environment and the operating conditions.

Influence of the Environment

A device placed in a given environment is subjected to its effects. The main environmental factors that accelerate device aging are:

  • Temperature

  • Percent load

  • Relative humidity

  • Salt environment

  • Current harmonics

  • Dust

  • Corrosive atmosphere

  • Vibration

  • Operating cycles

  • Interrupted currents

The tables in this chapter summarize for each factor:

  • Why it is harmful: influence

  • How to identify it: appearance

  • Impact on operation: consequences

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?