How to Maintain MicroLogic XMicroLogicMicroLogic Active Control Unit

@TW: profiled topic used in Maintenance Guides: DOCA0305 (MTZ with Mic Act), DOCA0099 (MTZ with Mic X), LVPED508016 (NT/NW)

Functions

The control unit permanently monitors the electrical network and generates trip orders when electrical faults are detected.

Electronic component qualification data is usually quoted for a 10-year lifetime by the component suppliers according to the device mission profile. The control unit can operate more than 10 years, depending on the operating environmental conditions (for example, temperature, humidity, vibrations, mechanical shocks, corrosive atmosphere).

Schneider Electric recommends that the Schneider Electric Services representative replaces the MicroLogic X control unit and associated optional ESM or M2C modules every 15 years. Each time the MicroLogic X control unit is replaced, the performer, the rating plug, and the sensor plug must be replaced by the Schneider Electric Services representative.

Electronic component qualification data is usually quoted for a 10-year lifetime by the component suppliers according to the device mission profile. The control unit can operate more than 10 years, depending on the operating environmental conditions (for example, temperature, humidity, vibrations, mechanical shocks, corrosive atmosphere).

Schneider Electric recommends that the Schneider Electric Services representative replaces the MicroLogic control unit and associated optional M2C modules every 15 years. Each time the MicroLogic control unit is replaced, the performer, the rating plug, and the sensor plug must be replaced by the Schneider Electric Services representative.

Electronic component qualification data is usually quoted for a 10-year lifetime by the component suppliers according to the device mission profile. The control unit can operate more than 10 years, depending on the operating environmental conditions (for example, temperature, humidity, vibrations, mechanical shocks, corrosive atmosphere).

Schneider Electric recommends that the Schneider Electric Services representative replaces the MicroLogic Active control unit every 15 years. Each time the MicroLogic Active control unit is replaced, the performer plug and the sensor plug must be replaced by the Schneider Electric Services representative.

Firmware Update Policy

@TechPub writer (07/2018): text in this block is copied from DOCA0155EN (Micrologic Trip and Control Units - Firmware History - Release Note) block “Firmware Upgrade Policy”. To update accordingly in future releases.

The MicroLogic X control unit is the main component of the intelligent modular unit (IMU).

The primary reason for updating the firmware of a MicroLogic X control unit is to obtain the latest IMU features. If the latest IMU features are not required, it is not mandatory to update the firmware of the MicroLogic X control unit and the Enerlin’X devices of the IMU.

Use the latest version of EcoStruxure Power Commission software to update the firmware of the MicroLogic X control unit or an Enerlin’X device of the IMU.

After updating the firmware of one device, Schneider Electric recommends that you update the firmware of the other devices in the IMU to keep consistency and avoid discrepancies between devices. Before proceeding, check the compatibility of the other devices with the new firmware.

For more information about firmware update policy, refer to MicroLogic Trip Units and Control Units - Firmware History.

Firmware Update Policy

The primary reason for updating the firmware of a MicroLogic Active control unit is to obtain the latest MicroLogic Active features. If the latest MicroLogic Active features are not required, it is not mandatory to update the firmware of the MicroLogic Active control unit.

Use the latest version of EcoStruxure Power Commission software to update the firmware of the MicroLogic Active control unit.

For more information about firmware update policy, refer to DOCA0267•• MasterPacT MTZ - MicroLogic Active Control Unit - Firmware Release Notes.

Degradation Factors

The factors which can cause degradation of the control unit and electronic components are the following:

  • Shocks

  • Vibration

  • Humidity

  • High ambient temperature

  • Corrosive atmosphere

Potential Hazards

Performing regular maintenance on the control unit can help to avoid the potential hazards and consequences listed in the following table.

Hazard

Consequence

Personal injury

Equipment damage

High short-circuit current and no tripping order

Degradation of the breaking unit

Preventive Action

The following table lists the preventive maintenance procedures to be performed to maintain the control unit.

Maintenance program

Preventive action

Procedure

Routine end-user preventive maintenance

Check the general condition of the device.

Device NII_Z_1

Device NII_1_1

Device NII_ZA_1

Intermediate end-user preventive maintenance

Check overcurrent protection.

Control Unit NIII_Z_4

Device NIII_2_1

Device NIII_ZA_4

Manufacturer preventive maintenance

Perform aging diagnostic to evaluate when to preventively replace the MicroLogic XMicroLogicMicroLogic Active control unit.

Contact your Schneider Electric Services representative.

For more information, refer to Preventive Maintenance Programs.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?