Influence of Harmonics on Aging

@TW: used in Maintenance Guides: DOCA0305 (MTZ with Mic Act), DOCA0099 (MTZ with Mic X), LVPED508016 (NT/NW)

Harmonics

Influence

Appearance

Consequences

Increase in skin effect, proximity effect, iron loss, Foucault/Eddy currents

  • Change in color of terminals, insulators, and grease

  • Modified display of LCDs

Harmonics cause temperature rise greater than that of the fundamental current

Possible overload of neutral if third-order harmonics and their multiples are present

Distorted waveform

  • Erroneous current value

  • Nuisance tripping if non-rms control units

Recommendations

The maintenance and installation recommendations according to the harmonics are defined in the following table:

THDi in % of In

Description

Maintenance recommendations

Installation recommendations

≤ 30 %

No notable influence on aging.

Implement the Intermediate program.

No particular recommendation

30 % to 50 %

At 40 % THDI, potential heat generation is approximately 10 % higher, corresponding to 5 % more current.

Carry out more frequent periodic checks.

Standard filtering with an inductor to reduce harmonics

> 50 %

Carry out more frequent periodic checks.

If necessary:

  • Oversize the neutral

  • Oversize switchgear

  • Filtering is mandatory

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?