Influence of Operating Cycles on Aging

@TW: profiled topic used in Maintenance Guides: DOCA0305 (MTZ with Mic Act), DOCA0099 (MTZ with Mic X), LVPED508016 (NT/NW)

Number of Operating Cycles

Influence

Consequences

The number of operating cycles depends directly on the electrical and mechanical endurance of the device.

Device service life depends on the daily number of operating cycles.

Example: Influence of operating cycles on the service life for a MasterPacT MTZ2MasterPacT NT/NWMasterPacT MTZ2 2000 A device.

Number of cycles

Service life (1)

30 cycles per month, or one cycle per day

27 years

60 cycles per month, or two cycles per day

13 years

120 cycles per month, or 4 cycles per day

6 years

(1) Service life is defined for endurance of 10,000 cycles and an interrupted current of less than 0.4 In

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?