Influence of Vibration on Aging

@TW: used in Maintenance Guides: DOCA0305 (MTZ with Mic Act), DOCA0099 (MTZ with Mic X), LVPED508016 (NT/NW)

Vibration

Influence

Appearance

Consequences

Premature deterioration of contact surfaces (clusters and main contacts)

Not identifiable

Increased device temperature rise

Loosening of bolted assemblies

Not identifiable

Increase in mechanical play

Wear of mechanical parts

Not identifiable

Broken springs. Increase in mechanical play between parts

Appearance of fretting corrosion on auxiliary connections

Not identifiable

Erroneous information or interruption of continuity in data or supply, excessive temperature rise

Breaking of connectors on large electronic components (for example, large capacitors)

Not identifiable

Potential failure of protection function

Recommendations

The maintenance and installation recommendations according to the vibrations are defined in the following table:

Thresholds (g)

Description

Maintenance recommendations

Installation recommendations

≤ 0.2 g

Normal condition, no impact on service life

Implement the Intermediate program.

No particular recommendation

0.2 g to 0.5 g

Reduced service life

Carry out more frequent periodic checks.

No particular recommendation

0.5 g to 0.7 g

Significant increase in incidents

  • Carry out more frequent periodic checks.

  • Check in particular the tightness of connections.

Install switchgear on a rubber mounting bushing

≥ 0.7 g

Forbidden for standard devices

Use special devices

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?