Service Selection

Class 2710 / Refer to Catalog 2700CT1101

Merchandised Speed-D Switchboards

Subfeed Circuit Breakers [1] [2]

Description

Rating
(A)

2-Pole [3]

3-Pole

Catalog No.

Catalog No.

Left

Right

Left

Right

Subfeed Circuit Breaker Kits
Includes circuit breaker, connectors and mounting hardware.

100

SASFB100L( )

SASFB100R( )

SASFB100L

SASFB100R

110

SASFB110L( )

SASFB110R( )

SASFB110L

SASFB110R

125

SASFB125L( )

SASFB100R( )

SASFB125L

SASFB125R

150

SASFB150L( )

SASFB150R( )

SASFB150L

SASFB150R

175

SASFB175L( )

SASFB175R( )

SASFB175L

SASFB175R

200

SASFB200L( )

SASFB200R( )

SASFB200L

SASFB200R

225

SASFB225L( )

SASFB225R( )

SASFB225L

SASFB225R

Footnotes

  1. Cannot use subfeed circuit breaker kit with multiple mains service section switchboards.
  2. For use on all Speed-D switchboards except Series E4.
  3. Two pole circuit breaker catalog numbers are completed by adding required phase connection letters as suffix (for example, SASFB100LAC).
Feedback