Ranges Pin Configuration Output Type Rated Current Functions Function Descriptions For detailed function definitions, see Timer Function Description. Catalog Number 24–240 Vac/Vdc 1.2 s to 300 h 8–Pin Octal DPDT Relay 5 A A Power On delay RE48ATM12MW A1, A2, H1, H2 Delay On Energization, Pulse-on
Section 16: NEMA and Definite Purpose Contactors and Starters
DSO 30–50 Full Load Amperes Type DPSG—2 and 3-Pole 30–40 Full Load Amperes Ratings—Overload Contacts and Auxiliary Contacts Device VoltsAC Pilot Duty – AC Only(35% Power Factor) ContinuousCurrent Rating Make Carry and Break 9998 SO19999 SO49999 R20 & R219999 D10, D01,D11 & D20 120 or Less