7400CAOSHPDABC Resin encapsulated, buck boost transformers Style A, B, C 7400CAOSHPDDH Ventilated Type EE, drive isolation, auto-transformers Style D, H 7400CAOSHPDF Low voltage 750 and 1000 kVA Type EE Style F 7400CAOSHPDJ Ventilated Type EX Style J 7400CAOSHPDK Ventilated Type EX Style K 7400CAOSHPDKO Ventilated Type EX, wall-mounted using Square D brackets Style K with WMB 7400CAOSHPDMPZB Mini Power Zone Bolt-on A, AA, B, BB, C, CC
no charge) (for example, order as 8810UCG1V02S).208240 —480600Specify —110—220 380440550Specify V01V02V08V03 V05V06V07V99 For voltage codes used with control transformers, see Factory Modifications (Forms). Form S (separate control) is used when a separate source of power is available for the control
separately To order branch circuit breakers, see QO Plug-On Circuit Breakers) Hub Type (Order separately To order hubs, see Accessories and Hubs for CSEDs) Line SideMain LugsAWG/kcmil(Al/Cu) ServiceGroundLug|AWG/|kcmil|(Al/Cu) Bus Rating WeightEach(Lbs)and PalletQty. 2P Circuits (Max.) Type (Order