With Retaining Kit QO2DTI mechanical interlock attachment with retaining kits for securing two adjacent back-fed circuit breakers in dual power supply applications. Can be used with (2) 2Ps or (1) 2P and (1) 1P QO circuit breakers in QO816L100 load centers. QO2DTIM DE2E OBS This product is obsolete
. Start-Stop 1, 4, 12 A X X X X X X X Selector Switches Hand-Off-Auto 1, 4, 12 C X X X X X X X On-Off 1, 4, 12 C6 X X X X X X X Pilot Lights (specify color) For pilot light details, refer to the pilot light table in Digest Section 16. One light On 1, 4, 12 P X X X X X X X Separate Control Circuit As