-Line—Maximum P or R-frame branch circuit breaker 9.25 inches 10.25 inches Space Heater Enclosure, interior and trim ship fully assembled. 120 V is standard. Top feed applications only. NQ and NF require 18 inches equipment space in NEMA 3R/12 constructions.NQ and NF require 6 inch bottom end gutter in
N2 and Apogee P1 communication protocols. LonWorks™ is available in an option card. Altivar 212 Selection AC Input LineVoltage Three-PhaseMotor Power These horsepower, wattage and continuous ampere ratings apply to the default switching frequency and maximum 40 °C ambient. Refer to the installation