Inspection and Maintenance
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, or Arc Flash
Failure to follow these instructions will result in death or serious injury.
|
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, or Arc Flash
Failure to follow these instructions will result in death or serious injury.
|
Set environmental controls (thermostat, humidistat, other items.) to mitigate condensation (including times when the equipment is lightly loaded, such as storage, downstream loads deenergized). Consult the engineer of record for the appropriate environmental control settings.
Perform inspection and maintenance of the walk-in enclosure based on environmental conditions and experience. Abnormal operation or conditions may require immediate corrective action.
The inspection of the Masterclad Metal-Clad 27 kV Indoor Switchgear is outlined in detail in Instruction Bulletin 6055–40.
The following instructions apply only to the walk-in enclosure.
Routine Inspection
During regular inspection intervals, inspect for the following:
-
Check for leaks in the front aisle, in each cable compartment, and in the roof of the indoor switchgear. Check the roof, using a flashlight, through the vent openings from the front aisle. If large puddles of water are found at the doors, check the door gaskets.
-
Check the weeping holes in the cable compartment doors to make sure they are not clogged.
-
Check the heater and fan in the front aisle for proper operation. Check the thermostat settings (see Electrical Low Voltage Connections). Verify that the space heaters in the switchgear are operating.
-
Check that the door panic latch (for use in an emergency) is working properly.
Replacing the Air Filters
Replace air filters every six months or as environmental conditions dictate. The following table lists correct filter applications.
Air Filter Part Numbers
|
Filter Location* |
Bay Width in. (mm) |
Schneider Electric Part Number |
Size |
|---|---|---|---|
|
New Rear Door Top Louvers (see Rear Doors, Front (left) and Back (right)) |
36 (914) |
JYT25926 |
29.75 x 7.6 |
|
New Rear Door Bottom Louvers (see Rear Doors, Front (left) and Back (right)) |
36 (914) |
JYT16426 |
29.75 x 14.42 |
|
Rear Door |
22 (559) |
46005-679-01 |
11 x 13 |
|
36 (914) |
46005-243-01 |
11 x 19.5 |
|
|
Rear Eaves |
22 (559) |
44005-679-02 |
3.3 x 20 |
|
36 (914) |
46005-243-03 |
3.3 x 34 |
|
|
48 (1219) |
46005-418-02 |
3.3 x 46 |
Bottom Rear Door Filters
Instructions for changing the filter in the bottom of the rear door (item A in the figure above):
-
Open the rear doors.
-
Remove the four filter support nuts and the support (JYT22125) as shown in Removing the Used Filter (Bottom Louver). (Note: it is not necessary to remove the eight self-threaded screws in the support frame.)
-
Remove the used filter and discard it.
-
Replace the used filter with a new Schneider Electric filter (JYT16426).
-
Reinstall the filter support (JYT122125) along with the new filter.
-
Reinstall all the nuts and washers as shown in Replacing the New Filter (Bottom Louver).
Top Rear Door Filters
Instructions for changing the filter in the top of the rear door (item B in Walk-in Units with Rear Doors Open):
-
Open the rear doors.
-
Remove the four filter support nuts and the support (JYT25917) as shown in Removing the Used Filter (Top Louver).
NOTE: It is not necessary to remove the eight self-threaded screws in the support frame. -
Remove the used filter and discard it.
-
Replace the used filter with a new Schneider Electric filter (JYT25926).
-
Reinstall the filter support (JYT25917) along with the new filter.
-
Reinstall all the nuts and washers as shown inReplacing the New Filter (Top Louver).
DANGER