Introduction
This bulletin explains how to install a control bus, which is used to connect the Powerlink remotely operated circuit breakers and the Powerlink electronics.
Components of a Control Bus
The Powerlink system uses one or more NF Powerlink control busses attached to interior rails in a panelboard. The control busses are used only with NF panelboards manufactured August 1, 2000 or later because these panelboards have holes on the interior rails for mounting Powerlink control busses. The date code is located on a yellow sticker on the deadfront and also on the UL label located on the interior rail. The first number represents the year, the second number represents the week of the year, and the third number represents the day of the week (Monday = 1, Tuesday = 2, Wednesday = 3, etc.). NF panelboards with a date code of 00 31 2 or later are furnished with the above referenced mounting holes.
A control bus has a series of bus connections, or poles, which varies in number and is selected based on the size and type of the panelboard. Every control bus has a section containing one secondary bus interconnect cable connection, three LEDs, and vertical bus connections (see Figure 1). The vertical bus connections are used to connect the power supply, controller, or the secondary address selector accessory.
When installing control busses in a standard NF panelboard, there will be both left and right control busses. On an eighty-four space panel there are up to four control busses. The size of the panelboard used will determine the control bus size, and the number of poles will determine whether installation of both left and right control busses is needed (see Table 1 or Table 2). The left control bus is mounted to the left interior rail, while the right control bus is mounted to the right interior rail.
For a column-width panelboard, both control busses are mounted to the same interior rail. The left control bus is inverted and mounted at the bottom of the interior rail, while the right control bus is mounted at the top.
Control Busses for Standard NF Panelboards
Panelboard Interior Size | Total Powerlink Pole Spaces | Available Powerlink Pole Spaces | Control Bus Catalog Number | Mounting Location |
---|---|---|---|---|
30 circuit | 24 | 12 or less | Left | |
13–24 | Left | |||
Right | ||||
42 circuit | 36 | 18 or less | Left | |
19–36 | Left | |||
Right | ||||
54 circuit | 42 | 21 or less | Left | |
22–42 | Left | |||
Right |
Control Busses for Column-width NF Panelboards
Panelboard Interior Size | Total Powerlink Pole Spaces | Available Powerlink Pole Spaces | Control Bus Catalog Number | Mounting Location |
---|---|---|---|---|
30 circuit | 24 (30)* | 12 or less | Top | |
18 or less | Top | |||
21 or less | Top | |||
22–24 | Top | |||
Bottom | ||||
(22–30)* | (Top)* | |||
(Bottom)* | ||||
42 circuit | 36 (42)* | 12 or less | Top | |
18 or less | Top | |||
21 or less | Top | |||
22–36 | Top | |||
Bottom | ||||
(22–42)* | (Top)* | |||
(Bottom)* |
LED Function and Operation
The three LED lights on a control bus indicate various network communications (see Figure 2). The LEDs are different colors and blink when data has been received or transmitted and whether the processor is active and functioning. LED Activity lists the LEDs and how they function.
LED Activity
LED | Color | LED Activity |
---|---|---|
RX | Green | When flashing, it indicates that data is being received. |
TX | Yellow | When flashing, it indicates that data has been received and a response has been sent. |
CPU | Red | When flashing concurrently with the RX LED, it indicates that the processor is active and data has been received. |
If the CPU LED flashes a steady on/off pattern with 0.5 seconds between each flash, the control bus is not receiving data. |