Installing the Control Bus
Follow these instructions to install the control bus into a panelboard. The installation is illustrated in Figure 3. If installing the control bus into a column-width panelboard, refer to Column-width Control Bus Installation.
![]() |
---|
hazard of electric shock, explosion, or arc flash
Failure to follow these instructions will result in death or serious injury.
|
WARNING: This product can expose you to chemicals including nickel compounds, which are known to the State of California to cause cancer, and Bisphenol A (BPA), which is known to the State of California to cause birth defects or other reproductive harm. For more information go to www.P65Warnings.ca.gov. |
-
Disconnect all power to the panelboard.
-
Remove the panelboard cover and deadfront. Verify that all power is off using a properly rated voltage sensing device.
-
Remove all branch circuit breakers (not required).
-
Position the left control bus so its mounting feet are aligned with the holes on the left interior rail in the panelboard. Notice that the vertical bus connections for the power supply are at the top of the control bus (see Figure 3).
-
Secure the mounting feet to the interior rail using the screws provided and a screwdriver. Torque the screw 20 to 30 lb-in.(2.3 to 3.4 N•m), then verify that the control bus is securely mounted to the interior rail and does not move or slide on the rail.
-
If a right control bus is needed, position it so the mounting feet are aligned with the holes on the right interior rail in the panelboard. Notice that the vertical bus connections for the controller are at the top of the control bus.
-
Secure the mounting feet to the interior rail using the screws provided and a screwdriver. Verify that the control bus is securely mounted to the interior rail and does not move or slide on the rail.
-
Proceed with the installation of Powerlink remote-controlled circuit breakers, controller, or power supply as indicated in related installation information. If finished with the installation, replace the deadfront and panelboard cover, and turn on the power.
Column-width Control Bus Installation
Follow these instructions to install the control bus into a column-width panelboard. The installation is illustrated in Control Bus Installation in a Column-width Panelboard.
![]() |
---|
hazard of electric shock, explosion, or arc flash
Failure to follow these instructions will result in death or serious injury.
|
-
Disconnect all power to the panelboard.
-
Remove the panelboard cover and deadfront. Verify that all power is off using a properly rated voltage sensing device.
-
Remove all branch circuit breakers.
-
Position the right control bus so its mounting feet are aligned with the holes on the interior rail near the top of the column-width panelboard. Notice that the vertical bus connections for the controller are at the top of the control bus.
- Use a screwdriver to secure the mounting feet to the rail using the screws provided. Torque the screw 20 to 30 lb-in. (2.3 to 3.4 N•m), then verify that the control bus is securely mounted to the rail and does not move or slide on the rail.
- Position the left control bus so the mounting feet are aligned with the holes on the interior rail in the panelboard. Notice that the vertical bus connections for the power supply are at the bottom of the control bus.
- Secure the mounting feet to the interior rail using the screws provided and a screwdriver. Verify that the control bus is securely mounted to the interior rail and does not move or slide on the rail
- Proceed with the installation of Powerlink remotely operated circuit breakers, controller, and power supply as indicated in the related installation information. If finished with the installation, replace the deadfront and panelboard cover, and turn on the power.