DUG_Wiser Micro Module Switch_PDL-00

Changing the device icon

You can change the device icon using the Wiser app.
  1. On the Home page, select the device for which you wish to change the icon.
  2. At the top-right corner of the screen, tap .
  3. Tap edit next to the device name.
  4. Tap Icon to view the menu.
  5. In the slide-up menu, select any one of the following (A) to change the device icon:
    • Take photo - allows you to take a photo with your device camera.
    • Select from Icon Library - allows you to select an icon from the app library.
    • Select from Album - allows you to select a photo from the mobile gallery.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?