DUG_Wiser Micro Module Switch_PDL-00

Manual operation

When the module is connected to a mechanical push button, the connected devices can be controlled manually by short pressing the push button.

NOTE: When the module is installed inside the wall box, the status LED is not visible while using the module.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?