Lock / unlock

Lock enables you to set the meter screen to default screen. You can scroll to other display screens while a screen is locked. Once the manual scrolling is stopped, the meter displays the default (lock) screen after 4 minutes.

Locking / unlocking meter screen

The meter’s display screen and buttons allow you to lock or unlock any screen.

Press and hold the Up and Down buttons simultaneously for 2 seconds to lock or unlock a meter screen.

NOTE:

You can only lock the display parameters. You cannot enter the Setup or Reset when a meter screen is locked.

You cannot enter the Setup or Clear when a meter screen is locked.

Button functions in locking / unlocking meter screen

Mode Button Function
Lock / Unlock Press and hold the Up and Down buttons simultaneously for 2 seconds to lock or unlock a meter screen.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?