Firmware version, model, and serial number

You can view the meter’s firmware version, model and serial number from the display panel. You can view the meter’s firmware version, model and serial number from the display panel, refer toDiagnostics page
  1. From the Home page, use Up or Down button to navigate to Maintain.
  2. Press OK.
  3. Use Up or Down button to navigate to Diag.
  4. Press OK.
  5. Meter display shows all LED turned on.
  6. Press Down button to view meter model, serial number, OS version, and RS version.
  7. Press Left button to exit Diag page.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?