THD% page

The meter provides complete harmonic distortion metering, recording, and real-time reporting, up to 15th harmonic for all voltage and current inputs (depending on the selected wiring configuration).

The following power quality measurements are available in the meter:

  • Total harmonic distortion (THD%) for current and voltage ( line-to-line or line-to-neutral, based on selected wiring configuration)

To view THD % parameters:

  1. From the Home page, use Up or Down button to navigate to THD %.
  2. Press OK.
  3. Press the Up or Down button to navigate to the next THD % parameter.
  4. Press Left button to exit.
The navigation of THD% parameter

Name on display

Description

%V12, V23, V31

Voltage THD% for Voltage lines 12, 23, and 31 respectively

%V1, V2, V3

Voltage THD% for Voltage lines 1, 2, and 3 respectively

%A1, A2, A3

Current THD% for current lines 1, 2, and 3 respectively

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?