PM2125C PM2225C PM2225CR Status input (DI) applications

Status inputs are typically used for monitoring the status of external contacts or circuit breakers.

Status inputs are typically used for monitoring the status of external contacts or circuit breakers and multi-tariff applications.

The meter’s status inputs require either an external voltage source or whetting voltage (provided in the meter) to detect the status input’s ON/OFF state. The meter detects an ON state if the external voltage appearing at the status input is within its operating range.

Wiring the status inputs

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?