PM2125C PM2225C PM2225CR Relay output applications

Relay outputs can be configured to be used in switching applications, for example, to provide on/off control signals for switching capacitor banks, generators, and other external devices and equipment.

Wiring the two digital inputs and relay output

A

Overcurrent protective device

B

Relay 1 (70, 71), Relay 2 (73, 74)

C

Whetting output (56, 57)

D

Digital status inputs (40, 42, 57)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?