Meter Features
-
Self guided LCD display and navigation
-
Energy accounting and balancing
-
Measurement of both True PF and Displacement PF
-
Active, reactive, and apparent energy readings
-
Min/Max values of instantaneous parameters with timestamp.
-
Cybersecurity: The meter supports the disabling of RS-485 port through front panel keys to prevent unauthorized access. Toggle the RTU devices in case of limited availability of nodes in software system.
-
SnapShot: The meter features include snapshot, which captures values of average voltage, average current, total active power, and delivered energy based on configured time in HH.MM format.
-
Suppression current: This is the minimum current at which the meter starts functioning. The meter can be configured to disregard the measurement of induced / auxiliary load current in the circuit. The suppression current selection can be done through the front display and through communication. The suppression current range is from 5 mA to 99 mA. The meter shows measurement if applied value is above the suppression value. The default suppression current is 5 mA.
You can use the meter as a stand-alone device, but its extensive capabilities are fully realized when used as part of an energy management system.
For applications, feature details and the most current and complete specifications of the PM2200 meters, see the EasyLogic PM2000 series technical datasheet at www.se.comwww.usa.siemens.com/pds.